Technical FAQs

Ask a Question

Using Reporter to Access System Data with a Custom Database Name

Goals and Symptoms

Summary


  • The default name for the ION database is ION_Data. However, some users may have changed the name of this database. This article explains the procedures necessary in order for you to view the data from this database using Reporter.

     

    Symptoms

    If the ION_Data database is not found when a query is added in Reporter, you are presented with the following window:

     


     

    However, after changing the Initial Catalog to match the real name of the database, the DSN for this database is not available in the Database Query Properties window.

     

Facts and Changes

Keywords
ION_Data

Database name

Initial catalog

Reporter

Causes and Fixes

Cause
The registry key IONInitialCatalog is set to ION_Data when installing ION Enterprise.

 

Resolution

Change the registry key IONInitialCatalog:

 

1. Go to Start -> Run.
2. Type regedit and press ENTER.
3. Go to HKEY_LOCAL_MACHINE \SOFTWARE\Power Measurement\ION Enterprise\5.0\Databases.
4. Double-click on IONInitialCatalog.
5. Change the value data to match the name you are using for the ION database.

 

Original article#10768


Legacy KB System (APS) Data: RESL182934 V1.0, Originally authored by DaMi on 03/20/2007, Last Edited by DaMi on 03/20/2007
Related ranges: ION Enterprise
Was this helpful?
What can we do to improve the information ?