Technical FAQs

Ask a Question

Updating the changes to the Flag colours for different users in Vista

Goals and Symptoms

Summary


  • If Vista has two or more users / logins, the changes made to the flag colours in the Vista diagram from one user / login are not reflected or updated in the other users /logins. This article explains how to carry forward or update these changes from one user login to the other

     

    Keywords

    Vista

    Flag colour

    Users

    Logins

     

    Symptoms

    One can go into Vista and set the flag colours (High, Low and Stale) for a numeric

     



     

    object as shown in the above diagram. However the changes made by a user, say Supervisor are not carried forward when any other user logs on to the same diagram. This can be more confusing when you create a new user, say UserViewOnly with View Only access level. Now we cannot make any changes to the Vista diagram for this user (in View Only access level), and so the flag colours will be different from the ones in the diagram as designed by the Supervisor.

     



     

    This can be advantageous as well as disadvantageous.

     

     

     

Facts and Changes

Keywords

  • Vista

    Flag colour

    Users

    Logins

Causes and Fixes

Cause
When we create a new user from Management Console, and when the new User logs into Vista for the first time, it generates an XML config file <username>.wsu which is used by the application. A copy of it is placed in text format in the folder:

D:\Program Files\PowerMeasurement\IONEnterprise\config\cfg\ud

 

This file contains the attributes for the flag colours: <LowFlagColor>, <HighFlagColor> and <StaleFlagColor>. When a new username.wsu file is created, the attributes take the default values / settings, which are

<LowFlagColor>#0000ff</LowFlagColor>

<HighFlagColor>#ff0000</HighFlagColor>

<StaleFlagColor>#ffff00</StaleFlagColor>

 

#0000ff Implies Blue

#ff0000 Implies Red

#ffff00 Implies Yellow

 

Workaround

The workaround here is to replace the above default attributes from the username.wsu file with those of the Supervisor.wsu file.


Document Change History

Date and Initials Comments
2010-03-16 DRM * Article maintenance according to feedback received.
  •  
    Original article#12753
    All content © 1992-2007 Schneider Electric

     


Legacy KB System (APS) Data: RESL182366 V2.0, Originally authored by DaMi on 02/27/2007, Last Edited by DaMi on 03/17/2010
Related ranges: ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?