Technical FAQs

Ask a Question

What is included in the Twido Modular Starter Pack - part number TWDXDPPAK2E?

The Twido Modular Starter Kit, P/N: TWDXDPPAK2E includes:

  • Twido Modular 20 I/O (12 24 V inputs, 8 24 V static outputs)
  • Display unit
  • Real-time clock module
  • Second serial port
  • 3-meter cable
  • Twido Soft programming software
  • Twido Training software

Legacy KB System (APS) Data: RESL2559 V1.0, Originally authored by on , Last Edited by on
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?