Technical FAQs

Ask a Question

What is the reason for the “Selected targetsystem mismatch with the connected device” message when you try to connect to a M238, M258 or LMC058 controller with SoMachine?


  • 1. The controller selected in the SoMachine software is not the same with the one used to connect. Verify the part number and change the controller in SoMachine.
    • If the controller has an S0 at the end of the part number you need to have the Solution Extension DVD installed on your computer to be able to select that controller.
    2. The firmware level is different. You need to upgrade the controller’s firmware.
Was this helpful?
What can we do to improve the information ?