Technical FAQs

Ask a Question

How to restart ProWORX 32 if it locks up.

Goals and Symptoms

How to restart ProWORX 32 if it locks up.

Facts and Changes

ProWORX 32

Causes and Fixes

If ProWORX 32 is locked up, it can be closed by using the following steps:

  • Open the Windows Task Manager.
  • Locate the task named 'ProWORX32.exe' and click on it.
  • Click on the 'End Process' button.
  • Click on 'Yes' in the 'Task Manager Warning' window.
  • Repeat the last three steps for the processes named 'PRWXPLCHolder.exe'
  • If you are using the ProWORX 32 server, repeat the above steps for the process
named 'PrwxCSHolder.exe' .
  • Start 'ProWORX 32'.
Was this helpful?
What can we do to improve the information ?