Technical FAQs

Ask a Question

The 'IO Drawing Generator' creates the AutoCad drawing for the 'DDM390-00' module with incorrect IO register numbers.

Goals and Symptoms

The 'IO Drawing Generator' creates the AutoCad drawing for the 'DDM390-00' module with incorrect IO
register numbers.

Facts and Changes

'ProWORX 32version 2.1, SP1A'

Causes and Fixes

The 'IO Drawing Generator' creates the AutoCad drawing for the 'DDM390-00' module with incorrect
IO register numbers.

The following steps can be used to resolve the problem:

  • Unzip the attached file.
  • Copy and replace the 'DDM390-00.DXF' drawing that is found in the 'ProWORX 32'\Drawings\Jic
folder with the one from the attached 'DDM390-00'.zip file.
  • Copy and replace the 'DDM390-00.DXF' drawing that is found in the master drawing folder
(i.e., C:\ProWORX 32\32\Drawings\Master ) with the one from the zip file.
  • Delete any drawings that were created for the module from both the intermediate and final
drawing folders.
  • Recreate the IO drawing using the 'IO Drawing Generator'.

Attachments

(Removed File URL: 200423_D066/DDM390-00.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/92efb20c3e3e5283c1257672001637a3/fl_block_5/0.5D0?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL200423 V1.0, Originally authored by AlCh on 11/18/2009, Last Edited by AlCh on 11/18/2009
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?