Technical FAQs

Ask a Question

"The Modbus Driver installation has failed.." error is returned during the update installation.

Goals and Symptoms

"The Modbus Driver installation has failed. Software installation has been cancelled" error mesage gets
returned

Facts and Changes

Advantys Configuration Software version 4.0

Causes and Fixes

If the "The Modbus Driver installation has failed. Software installation has been cancelled" error mesage
gets returned during the update installation of the Advantys Configuration Software, the issue can be resolved by
using the following steps.

  • Open the CD folder.
  • Open the 'Setup' folder.
  • Double click on the 'Advantys Setup' icon.
  • Click on 'Repair'
  • Click on 'Next' to start the update installation.

Legacy KB System (APS) Data: RESL192943 V1.0, Originally authored by AlCh on 01/08/2009, Last Edited by AlCh on 01/08/2009
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?