Technical FAQs

Ask a Question

How do I wire a 2-wire transmitter to a STBACO0220 or a STBACO0120 analog current output module?

The following wiring diagram indicates how to wire a 2-wire transmitter to the STBACO0220 or the STBACO0120 analog current output module as either a source or sink configuration. Loop supply voltage (+24vdc) is provided by the PDM. Note: The STBACO0120 is only a 1 channel module therefore the lower terminal connector will have no functionality.

    • Pin 1 +24VDC for sensor
      Pin 2 output to actuator
      Pin 4 output channel return
      Pin 6 +24VDC return

Legacy KB System (APS) Data: RESL180815 V1.0, Originally authored by DaSo on 12/05/2006, Last Edited by DaSo on 12/05/2006
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?