Technical FAQs

Ask a Question

STBNIP2212 Ethernet NIM Web Page Exec. Upgrade to v.1.14.2

Goals and Symptoms

The purpose of this Resolution is to inform Advantys users that the Ethernet NIM Web page Exec has been updated to version 1.14.2.

  •  

Facts and Changes

Upgrading the STBNIP2212 Ethernet NIM web pages to version 1.14.2 adds support for the following modules:

  • STBACI0320
  • STBACI8320
  • STBACO0220

Causes and Fixes

The attached zip file contains:

  • The web page 'Upgrade Procedure'
  • Upgrade.exe application file
  • Web file: web_files.zr

Please read the 'Upgrade Procedure' before attempting to load the web file.

Attachments

(Removed File URL: 177103_B442/stbnip2212_web_1142.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/ab2eb1682f1abf64c1257150004f8903/fl_block_5/0.5BE?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL177103 V2.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?