Technical FAQs

Ask a Question

What are the features of the Advantys STB NIM (Network Interface Module)?

The Advantys NIM is a multifaceted and necessary part of every island bus. It provides:

  • the gateway between the I/O on the island and the fieldbus master.
  • the interface for the Advantys configuration software.
  • a built-in power supply that provides logic power to I/O modules in the primary segment.

Legacy KB System (APS) Data: RESL164522 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?