Technical FAQs

Ask a Question

Does the 8030ICM200 include cables with purchase of the unit?

Yes. The 8030ICM200 includes the following cables with purchase of the unit:

  • a RS-232 12" cable with DB-9 port for the PC (part number 30614-039-50A)
  • a "Y" shaped 12" cable with DIN connectors to power the unit from the PC's keyboard port (part number 30614-042-01A)
  • a RS-422 10 foot cable to connect to the SY/MAX processor's RS-422 port (part number 8010CC100)

Legacy KB System (APS) Data: RESL164415 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?