Technical FAQs

Ask a Question

Is there a way to configure the Reference Data Editor in Concept 2.6 to default to 'Animation On'?

In Concept V2.6 SR1 the RDE animation defaulted to 'Animation Off' automatically whenever a template was opened. Concept 2.6 SR1D introduces a new switch in the concept.ini file, where the customer can select the RDE startup default mode.The Concept.ini file is found in the Windows folder. Please add the following:

    • [RDE]
      ; StartWithAnimation=1: Start RDE-animation when opening a RDE-template
      ; StartWithAnimation=0: Do not start RDE-animation when opening a RDE-template (Default)
      StartWithAnimation=1

Legacy KB System (APS) Data: RESL161867 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?