Technical FAQs

Ask a Question

What communication protocols are supported on the G200?

DNP 3.0 (serial and tcp/ip), Modbus (serial and tcp/ip), IEC101

      • Note: Based on part number

Legacy KB System (APS) Data: RESL212275 V1.0, Originally authored by DaFr on 08/09/2013, Last Edited by DaFr on 08/09/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?