Technical FAQs

Ask a Question

What is the size of the inter conductor for the N-series recloser cables (38kV)?

This size will vary depending upon the rating of the conductors:


  • 1. 250A 80mm2
    2. 340A 120mm2
    3. 400A 180mm2
    4. 630A 240mm2
    5. 800A 400mm2

    These are shown in more detail in the attached guide.

    Olex cables.pdfOlex cables.pdf


Legacy KB System (APS) Data: RESL212274 V1.0, Originally authored by DaFr on 08/09/2013, Last Edited by DaFr on 08/09/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?