Technical FAQs

Ask a Question

How to access the default DNP 3.0 map for a Micom relay without connecting to the relay.

How to access the default DNP 3.0 map for a Micom relay without connecting to the relay.


  • 1. Install Micom S1 Studio, if it is not already installed.

    2. Install the Data Model for your relay, reference KB RESL209934 for details on this process.

    3. Open Micom S1 Studio and create a New System.



    4. Verify successful system creation:


    5. Open the DNP3 file for the relay
      • a. Click File > Open Default File > DNP3 File
    6. Select the relay that you would like to work with:


Legacy KB System (APS) Data: RESL209949 V2.0, Originally authored by DaFr on 12/10/2012, Last Edited by DaFr on 05/17/2013
Related ranges: MiCOM S1 Studio
Was this helpful?
What can we do to improve the information ?