Technical FAQs

Ask a Question

Starting Register number in Modbus Read functions

Goals and Symptoms

When performing Modbus read commands, it is important to apply the right starting register address in the read function. Otherwise, the wrong register will be accessed from the meter, giving unexpected data for the meter parameter being read.


  • Meter is functioning as expected. The front panel values for voltages and currents are within expected ranges for the system being monitored. However, modbus read functions from a master station (e.g. a PLC) give values that do not correspond to the front panel values.

Facts and Changes

Modbus, modbus rtu, function read, modbus map, holding register, staring register, function 03, modbus read packet

Causes and Fixes

Cause
One probable cause would be that, the modbus function read command is not pointing to the right registers. The modbus protocol requires an offset to be introduced in the starting register address when reading the slaves register.

Resolution

When reading the meter parameters, the Master must send the device a Read Holding Registers packet. This packet must specify a start register and the number of registers to read. When the function read is received, the slave responds with a packet containing the registers in the range defined in the read request.

However, consider the 3710 Modbus map, which states that according to the MODBUS protocol, in response to a request for address 4xxxx, the master reads register xxxx-1 from the slave (3710). For example, a request for register 40011 returns register 10 from the slave.

What does the above statement mean? Why is an offset required?

Holding registers, by default, are defined the 4xxxx range, the first holding register staring at 40001. The starting register in the read packet is, on the other hand, numbered from zero. Hence, the start register zero automatically points to holding register 40001, starting register one points to holding register 40002, etc. The fact that the first holding register is 40001 and not 40000 explains the offset that needs to be introduced in the starting register number.

Hence, considering the 3710 Modbus Map statement, if the Master needs to read register 40011, then the corresponding starting register that needs to be put in the read function would be 10 (0A hex) since register 40011 is the register 10 from the first holding register, 40001:
40001 > Start register 0
40002 > Start register 1
40003 > Start register 2
40004 > Start register 3
40005 > Start register 4
40006 > Start register 5
40007 > Start register 6
40008 > Start register 7
40009 > Start register 8
40010 > Start register 9
40011 > Start register 10

The Modbus Read Request Packet for a master reading 3 registers from a slave with unit ID 100 (64 Hex) and for starting register of 40011 should be:
 

Slave ID
Function
Start Register (40011)
# of Registers
CRC Checksum
64
03
00
0A
00032C3C


To summarize, when looking at a modbus map, the starting register number to be used in the read function:

Start Register = Modbus Register 40001.

 

Original article#12774

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188799 V1.0, Originally authored by KBAdPM on 11/03/2007, Last Edited by KBAdPM on 11/03/2007
Related ranges: Modbus / JBus
Was this helpful?
What can we do to improve the information ?