Technical FAQs

Ask a Question

Sepam SFT2841 v 10.0 software runs slow.

More Information:
This issue has only been seen when Schneider-Electric Driver Software is installed after the Sepam SFT2841 software. It installs Modbus drivers that can overwrite the existing Modbus driver. This can also cause additional Modbus Drivers to be installed. The SFT2841 software will appear to run slower when connecting to the Sepam 20, 40, or 80 relay through the front panel connection. After selecting connect in the software it will take over 1 minute before the window is updated. Switching between tabs in the setup mode will take 30 to 40 seconds to refresh. There have been some instances where other computer programs run slow when the SFT2841 is running slow.

Solution:
The solution is to uninstall the incorrect Modbus Driver and install the SFT2841 Modbus driver that is supplied with the SFT2841 installation. The version should be 1.5 or newer.
To uninstall the Modbus driver:

  1. Go to Start>Programs>Schneider Electric>Communication Drivers>Drivers Manager>Schneider Drivers Management Properties.
  2. Then select the Modbus Driver 1 and uninstall it.
  3. Then select install/update and browse to the setup.exe in the driver folder where the drivers are located. (typical location on the CD or drive = x:\The SFT2841V10\Driver\setup.exe)

AEDL3
  • Last Revised: September 7, 2007

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188117 V2.0, Originally authored by KBAdPM on 09/17/2007, Last Edited by DaMi on 04/22/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)
Was this helpful?
What can we do to improve the information ?