Technical FAQs

Ask a Question

Does the SEPAM Series 20, 40, 80 relay have event recording?

The SEPAM series 20, 40, 80 relay has event recording. The SFT2841 software can be used to configure the number of events.


  • Last Revised: August 26, 2007


    All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL187772 V2.0, Originally authored by PhHa on 08/27/2007, Last Edited by DaMi on 04/22/2008
Related ranges: Sepam series 80, Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?