Technical FAQs

Ask a Question

SMS 3.2 and later has problems with the Turtle Beach - Santa Cruz sound card under Windows NT 4.0.

Issue
SMS 3.x and later has problems with the Turtle Beach - Santa Cruz sound card under Windows NT 4.0 causing no alarms to be read from the devices in the system.

Product Line
SMS 3.x

Resolution

When the sound card driver is loaded, no alarms will be read from the devices in the system. This sound card is no longer supported by Turtle Beach under Windows NT 4.0. It will be necessary to unload the sound drivers.

Note: This sound card works correctly under Windows 2000.



 
  •  

    Internal PMO/PMC

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189575 V1.0, Originally authored by KBAdPM on 11/23/2007, Last Edited by KBAdPM on 11/23/2007
Related ranges: System Manager 3.2
Was this helpful?
What can we do to improve the information ?