Technical FAQs

Ask a Question

How can I change the default sounds for my onboard alarms in SMS-3000 series software.


The default sounds for onboard alarms is the same as the software alarm defaults.

1. Go to Setup>Functions/Alarms and select the Global Function tab.

2. Select any function that allows the use of the Setpoints button and click on the Setpoints button.

3. At the Edit Setpoints dialog box click on one of the Severity... buttons that is available.

4. Select the desired sound for the appropriate alarm level from the drop down menu, attached is the screen shot for reference

5. If custom sounds are desired then while still at the Severity dialog, click on Sounds, then on Add, then on Select. The custom sound can then be browsed for and selected.

6. Select OK/Close to back out of the dialogs.


    Original article#2404

    Internal PMO/PMC

    All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL186155 V1.0, Originally authored by KBAdPM on 07/04/2007, Last Edited by KBAdPM on 07/04/2007
Related ranges: System Manager 3.3
Was this helpful?
What can we do to improve the information ?