Technical FAQs

Ask a Question

What devices are compatible with the Sub Meter Display?

Issue
What devices are compatable with the Sub Meter Display?

Product Line
Sub Meter Display (SMD and SMDOPN)
MCM (Multi Circuit Meter)
Enercept Meter
BCM (Branch Circuit Monitor)

Environment
SMD Communications 

Cause
What devices are compatable with the Sub Meter Display (SMD)?

Resolution
The Sub Meter display (SMD) supports the following Modbus devices:

Enercept Meters
Branch Circuit Monitors (BCM42)
Multi-Circuit Monitors (MCM8364)
Alta Labs network Temperatures/Humidity  Sensors (HXO-485, TXO-485, HXO/T-485)

Was this helpful?
What can we do to improve the information ?