Technical FAQs

Ask a Question

What are the product standards for the CM4000?

Issue
The UL listing for the CM4000

Product Line
CM4000

Environment
Standard Compliance

Resolution
For safety, the CM4000 is UL 508 for the USA. It's listing is cUL and UL listed 18x5 Ind. Cont. Eq. This information is listed in the CM4000 IB under the specifications. This can be found on page 8 of the attached document

Was this helpful?
What can we do to improve the information ?