Technical FAQs

Ask a Question

How do you use a LiveLabel Applet?

Use one LiveLabelApplet for every symbol (variable) or direct-address
that you want to monitored on the Web page. For example, if you are monitoring three symbols
(variables), you would include the applet three times.
This applet displays the following three fields:
1) Field Description
2) Your label for the symbol (variable) or direct address
3) Run-time value of the symbol (variable) or direct address and the units you specify for the value.

HTML example of a LiveLabelApplet:
<APPLET codebase="/classes" archive="SAComm.jar"
code="com.schneiderautomation.factorycast.LiveLabelApplet"
width=300 height=30>
<PARAM name=LABEL value="Reactor 1 Temperature">
<PARAM name=UNITS value="F">
<PARAM name=ADDRESS value="40101">(ForPremium value="%MW100")
<PARAM name=DATATYPE value="UINT">
<PARAM name=FORMAT value="DEC">
<PARAM name=GAIN value="2.0">
<PARAM name=BIAS value="100.0">
<PARAM name=FOREGRND value="WHITE">
<PARAM name=BACKGRND value="BLACK">
<PARAM name=ERROR_COLOR value="RED">
<PARAM name=FONT_NAME value="SERIF">
<PARAM name=FONT_BOLD value="TRUE">
<PARAM name=FONT_ITALIC value="FALSE">
<PARAM name=FONT_SIZE value="10">
</APPLET>


Was this helpful?
What can we do to improve the information ?