Technical FAQs

Ask a Question

Can you have both the Data Watch Window and Register Editor visible at the same time in ProWORX 32 when online with a controller?

No. There is no way to get the Data Watch Window and the Register Editor to be visible at the same time when online to the controller because they both share the same window. The Data Watch Window when opened always replaces the Register Editor and vise versa.


Legacy KB System (APS) Data: RESL202672 V2.0, Originally authored by RoAl on 06/19/2010, Last Edited by RoAl on 12/05/2013
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?