Technical FAQs

Ask a Question

How do I stop the Navigation window from disappearing in the ProWORX 32 programming software?

To stop the ProWORX 32 Navigation window from disappearing, open the ProWORX 32 Properties window. Select the Environment tab, under the Environment option, uncheck the option for "Enable Scrolling Navigation Panel" and Apply. This will stop the Navigation window from disappearing.

Legacy KB System (APS) Data: RESL191733 V2.0, Originally authored by RoAl on 04/22/2008, Last Edited by RoAl on 01/26/2011
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?