Technical FAQs

Ask a Question

How many connections does the Vijeo Designer Web Gate support?

8 is the maximum number of connection supported by the Web Gate when using Vijeo Designer V4.6 or higher.


Legacy KB System (APS) Data: RESL188764 V1.0, Originally authored by MiMe on 11/01/2007, Last Edited by MiMe on 11/01/2007
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?