Technical FAQs

Ask a Question

What is the pinout of the integrated Serial port on the M340 PLC's BMXP34 1000/2010/2020?

The pinout of the integrated Serial port on the M340 PLC's BMXP34 1000/2010/2020 is:


Legacy KB System (APS) Data: RESL180821 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?