Technical FAQs

Ask a Question

Can I transfer a Vijeo Designer project to a XBTG via Ethernet if behind a firewall?

Yes. When the target machine and PC with Vijeo Designer software reside on opposite side of a firewall, you will need to configure the firewall.


Legacy KB System (APS) Data: RESL174243 V2.0, Originally authored by MiOB on 09/04/2013, Last Edited by GeMc on 09/04/2013
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?