Technical FAQs

Ask a Question

Does Schneider have a utility to compare two PL7 applications?

Yes. The utility used to compare two PL7 applications is called PL7DIF. The utility allows a comparison between two PL7 applications for Micro and Premium PLCs (in .STX format).
The reference number TLXCDPPL7DIF41.


Legacy KB System (APS) Data: RESL173524 V2.0, Originally authored by MiOB on 04/26/2013, Last Edited by GeMc on 04/26/2013
Related ranges: PL7
Was this helpful?
What can we do to improve the information ?