Technical FAQs

Ask a Question

What would cause not being able to select MB Plus for Port Device in the Port Parameter Tab of the Panelmate Plus Transfer Utility?

This is caused by the Modbus Plus flag not being set in the vcpxfer.ini file. To resolve the problem, edit the vcpxfer.ini file and change EnableModbusPort16=0 to EnableModbusPort16=1.


Legacy KB System (APS) Data: RESL173229 V1.0, Originally authored by on , Last Edited by on
Related ranges: Panelmate
Was this helpful?
What can we do to improve the information ?