Technical FAQs

Ask a Question

What causes a 'threed.vbx' file error when launching the ProWORX NxT software?

The 'threed.vbx' file error is generated if ProWORX NxT attempts to access a version of 'threed.vbx' other than the file created (7/17/93). This error will usually point to either the System or System32 folder on your PC. The correct 'threed.vbx' file is dated (7/17/93). ProWORX NxT was developed with this file, so you need this dated file for NxT to run properly. Do a search on your PC for the file with this date. If the file is found in a different folder, simply copy/paste it into the folder that contains the file with the incorrect date. If you don't have the (7/17/93) dated 'threed.vbx' file anywhere on your PC, then use the attached file below.

Was this helpful?
What can we do to improve the information ?