Technical FAQs

Ask a Question

Does the Recovery checkbox need to be selected when downloading the runtime to the Magelis XBT-G?

Goals and Symptoms

Does the Recovery checkbox need to be selected when downloading the runtime to the Magelis XBT-G?

Facts and Changes

No, the recovery option should not be selected when downloading the runtime to the Magelis XBT-G.
 

Causes and Fixes

The recovery option is only used to recover the Magelis XBT-G when the unit is locked up

(i.e., If the XBT-G has a limited amount of DRAM (e.g. 8MB) and a large application is downloaded to it, the application may not be able to run and the unit could locks up. If this occurs then the user would use the recovery to clear the XBT-G of the error that caused it to lock up. They would then correct the application to fit in the XBT-G and download it.)


Legacy KB System (APS) Data: RESL160997 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-L
Was this helpful?
What can we do to improve the information ?