Technical FAQs

Ask a Question

Is there a known problem assigning IP addresses to the Momentum ENT modules?

Yes, Some of the Momentum ENT modules have problems when trying to save their IP address to Flash. You can Identify if your ENT has this problem if the serial number of that module is in the range of 310132xxxxx to 310203xxxxx AND if you peel back a label that says REV xx on the PCB side and the chip has a you need to send that module in for an exchange. An executive has been developed to correct the problem for newly manufactured ENT's to be able to use both types of flash ram chips. If the chip inside has a symbol of then continue to use it. If your ENT does not have both of these descriptors as describe above then the IP address problem you are having is being caused by something else.

Was this helpful?
What can we do to improve the information ?