Technical FAQs

Ask a Question

Which Quantum PLCs allow the use of an Aux task in Unity?

The 140CPU65150, 140CPU65160, and 140CPU67160 allow the use of Aux tasks numbered 0 thru 3. The 140CPU31110, 140CPU43412A, and 140CPU53414A will only allow the use of a Fast and a Mast task.


Legacy KB System (APS) Data: RESL2568 V1.0, Originally authored by on , Last Edited by on
Related ranges:

AEDL3
Was this helpful?
What can we do to improve the information ?