Technical FAQs

Ask a Question

Which Quantum PLCs are supported in Unity Software?

The following PLCs are supported:
140CPU67160
140CPU65160
140CPU65150
140CPU31110
140CPU53414A*
140CPU43412A*
*These two controllers require a new Exec file to function with Unity


Legacy KB System (APS) Data: RESL2561 V1.0, Originally authored by on , Last Edited by on
Related ranges:

AEDL3
Was this helpful?
What can we do to improve the information ?