Technical FAQs

Ask a Question

What is State Ram?

State Ram, also known as State Memory or the Image Table, is a table in the PLC memory that contains the status of all inputs. It holds the references for
0X, 1X, 3X and 4X registers. Discrete inputs (contacts), discrete outputs/holding bits (coils), input registers and output registers/holding registers all make up state ram.

Was this helpful?
What can we do to improve the information ?