Technical FAQs

Ask a Question

How to modify the size of the Alarm and/or Activity logs in SMS

Goals and Symptoms

How to modify the size of the Alarm and Activity logs in SMS.

Causes and Fixes

From the SMS Setup utility, select Setup/Administrative/Alarm Activity logs


Legacy KB System (APS) Data: RESL212997 V1.0, Originally authored by MiZe on 11/13/2013, Last Edited by MiZe on 11/13/2013
Related ranges: System Manager 4.0, System Manager 4.2, System Manager 4.3
Was this helpful?
What can we do to improve the information ?