Technical FAQs

Ask a Question

How do I change the range on numeric dials in System Manager Software (SMS)?

The tick marks on the SMS meter gauge does not fit customers value.

System Manager Software (SMS) 4.0.x and above

SMS diagrams viewing meter gauges. 

The range on meter dials/gauges in SMS is set to a default value when added to a diagram.

To change the range on the meter displays open the "SMS Setup Utility > Setup > Devices/Routing > Ratings".

Select the desired meter display quantity from the available section and change the ratings value as desired
In the example below, the device rating is 200 and the dial maximum range is 200.

Note: This feature is only available in SMS 4.0.x and above.

Changing the value to 300, causes the dial maximum range to go to 300.

Legacy KB System (APS) Data: RESL212540 V1.0, Originally authored by MiZe on 09/19/2013, Last Edited by MiZe on 09/19/2013
Related ranges: System Manager 3.3, System Manager 4.3, System Manager 4.2, System Manager 4.0
Was this helpful?
What can we do to improve the information ?