Technical FAQs

Ask a Question

EM3500 driver isn't showing up in ION Setup.

Issue
When looking for EM3500 as a device type I cannot find it

Product Line
EM3500
ION Setup

Environment
Hardware drivers

Cause
Earlier versions of the software did not include the EM3500 meter

Resolution
Earlier versions of ION Setup do not come with the EM3500 driver. Buid version 3.0.13144 introduced the EM3500 driver. See the link below for a more recent version of ION Setup which will include the EM3500 driver.

http://www.schneider-electric.com/en/product-range-download/61461-ion-setup-3-0

Was this helpful?
What can we do to improve the information ?