Technical FAQs

Ask a Question

Why are dashes displayed instead of a value for demand power on my PM800 series meter?

The dashes will be displayed following a power cycle to the power meter.The meter must complete one demand calculation before a value is displayed. This time is directly dependent upon the demand interval. Once the demand interval is complete a value will be displayed. This may happen for any measurement that is computed using a time interval.


Legacy KB System (APS) Data: RESL212079 V1.0, Originally authored by DaFr on 07/17/2013, Last Edited by DaFr on 07/17/2013
Related ranges: PM800 series
Was this helpful?
What can we do to improve the information ?