Technical FAQs

Ask a Question

Powerlogic/ION meter comparison chart

Issue
Users may want to compare Schneider power meters

Product Line
 iEM 2000/iME, iEM 3000 series, BCPM, EM4000 series, PM8000 series, PM5000 series, PM700 series, ION6200, ION7300 series, ION8800, ION8650, ION8600, ION7550/ION7650, CM4000 series

Environment
Metering & Power Monitoring

Cause
Different meters have significantly varying features, and specifications have different requirements

Resolution
The meter resolution table lists the recent/current meter offering from Schneider Electric, and indicates differences between their various features.

Reference the following link for the meter comparison chart (Note the tabs at the top of the page, which switch between tables of feature type sets):
http://www.schneider-electric.com/documents/electrical-distribution/en/shared/PowerLogic/PowerLogic-meter-comparison.html

 
Was this helpful?
What can we do to improve the information ?