Technical FAQs

Ask a Question

The monitoring tab is grayed out on PM8ECC

Issue:
The monitoring tab is grayed out and can't be clicked.

Product Line
PM8ECC

Environment
Web Server

Cause:
The web page access to the web pages under the monitoring tab are either set to none or are removed from the page.



Resolution:
1. Change the web page access from None to either Read-Only or Full.
2. Add the web page back to the monitoring page by clicking the Add/Remove Web Pages button.

 

Was this helpful?
What can we do to improve the information ?