Technical FAQs

Ask a Question

Values not being displayed in Vista or Diagrams for BCPM in StruxureWare Power Monitoring (SPM) - "Unexpected ION exception code 'NotSupported' - Illegal Data Address"

Goals and Symptoms

Issue
When viewing data from a BCPM in StruxureWare Power Monitoring's Vista or Web Application's Diagrams the values are not displayed and the boxes are highlighted dark green/olive/brown color. When hovering your mouse cursor over the box, the follow message is displayed:

System error. The source returned an unexpected result. "Unexpected ION Exception code 'NotSupported' - Illegal data address."

Facts and Changes

Environment

SPM, PME, StruxureWare Power Monitoring, Power Monitoring Expert

Causes and Fixes

Cause

With firmware version 1.012 of the BCPM, the register mapping had some slight changes. Vista screens in StruxureWare 7 were updated to reflect these changes. Individuals who are running a earlier firmware version and StruxureWare 7.0 and later may see this issue.


Resolution

Upgrading the BCPM firmware to 1.012 or later will correct this issue. The latest firmware is available from powerlogic.com and DLF3000 is used to upgrade the firmware of the meter.


Legacy KB System (APS) Data: RESL211434 V1.0, Originally authored by MaTh on 05/11/2013, Last Edited by MaTh on 05/11/2013
Related ranges: BCPM(Branch Circuit Power Meter), Power Monitoring Expert 7
Was this helpful?
What can we do to improve the information ?