Technical FAQs

Ask a Question

Struxureware Power Monitoring 7.0.1 Installer fails with Return code 1645

Goals and Symptoms

Issue
Struxureware Power Monitoring 7.0.1 Installer fails with the following message during the "Copy Files" portion:

"Install Completed with error. Return code is1645"

Causes and Fixes

Cause

This error has been the result of installing SPM from media other than a local CD/DVD drive or local hard drive. (i.e. Shared network drive and/or portable USB CD/DVD drive).


Resolution

To resolve this issue copy the files from the SPM installation media to the local hard drive of the local server. Run the SPM 7.0.1 Installer from the local hard drive.


Legacy KB System (APS) Data: RESL211399 V1.0, Originally authored by MaTh on 05/09/2013, Last Edited by MaTh on 05/09/2013
Related ranges: Power Monitoring Expert 7
Was this helpful?
What can we do to improve the information ?