Technical FAQs

Ask a Question

What is the default IP address for the ION7300 series power meter?

The default Modbus TCP/IP settings for the ION7300 series meter are as follows:
IP Address = none
Subnet Mask = none
Gateway = none


Legacy KB System (APS) Data: RESL211344 V1.0, Originally authored by MaTh on 05/02/2013, Last Edited by MaTh on 05/02/2013
Related ranges: ION7300
Was this helpful?
What can we do to improve the information ?