Technical FAQs

Ask a Question

How to enable 100ms Frequency monitoring on a CM4000 series meter

Enabling 100ms frequency monitoring on a CM4000

Product Line

High Speed Monitoring

By default 100ms frequency monitoring is not enabled

100ms Frequency monitoring is disabled by default on the CM4000 series meters. To enable this feature, the following command writes must be executed to the meter:

Write 9020 to register 8000
Write 11 to register 3239
Write 1 to register 8001
Write 9021 to register 8000

This will enable 100ms Frequency monitoring. The value is stored in register 1080 (Units - 0.01 Hz).

Was this helpful?
What can we do to improve the information ?