Technical FAQs

Ask a Question

How do PowerLogic onboard alarm priorities correspond to StruxureWare Power Monitoring alarm priority levels?

Issue:
Many PowerLogic meters have onboard alarming functionality. Meter such as the PM800 (PM8), CM3000 (CM3), and CM4000 (CM4) series have 4 priority levels: high, medium, low and none. Power Monitoring Expert assigns each alarm a number, and users would like to know how the priority level translate to alarm priority numbers in SPM/PME.

Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0


Environment:
Power Monitoring Expert Web Applications Alarming

Resolution:
Below is how those priority levels are displayed in StruxureWare Power Monitoring (SPM or PME):
No priority - 64
Low Priority - 64
Medium Priority - 128
High Priority - 200

Was this helpful?
What can we do to improve the information ?