Technical FAQs

Ask a Question

Is it possible to change the High/Low/Stale/Error flag colors of Numeric Objects in Vista?

In Vista numeric objects have default colors assigned for high/low/stale/error flags. This can be customized by going to Options>Flag Colors in Vista.
Please refer to RESL188666, to change the flag color in Web Client of SPM 7.0.1 (Web Applications).

Environment
StruxureWare Power Monitoring, SPM, ION

Was this helpful?
What can we do to improve the information ?