Technical FAQs

Ask a Question

What is the EM4800 Pulse Out Connector?

User wanted to know if it is possible to use the Pulse Out Connector located on the EM4800

Product Line

Hardware Specifications

The EM4800 Installation Guide references a Pulse Out Connector located on the bottom right of the circuit board. The Pulse Out Connector shown below is not a customer usable interface. It has specific test conditions that are used for manufacturing and testing purposes. The EM4800 is not capable of sending a pulse output.

Was this helpful?
What can we do to improve the information ?