Technical FAQs

Ask a Question

Is the Ethernet Communication Module (ECM) compatible with StruxureWare Power Monitoring (SPM)?

Yes, The ECM is supported in SPM. The ECM uses the Modbus RTU/TCP protocol which is communicated over port 502.


Legacy KB System (APS) Data: RESL211142 V1.0, Originally authored by MaTh on 04/06/2013, Last Edited by MaTh on 04/06/2013
Related ranges: ECM (ECMRM / ECM2000)
Was this helpful?
What can we do to improve the information ?